我们今天能为您提供什么帮助?

Is the OFS Server V3.63 supported on Windows 11 operating system?

Issue:
OFS Server V3.63 supported on Windows 11 operating system


Product Line:
OFS server


Resolution:
Yes, but you will have to install SP2. Below is the link to download SP2 for the OFS server V3.63.
https://www.se.com/us/en/download/document/OFS_3_63_4904_SP2/