If you add the IP55 flange kit NSYPTDS5 to the ATV630 Drive, will it make the drive alone IP55 ratings.
Issue:
If you add the IP55 flange kit NSYPTDS5 kit to the ATV630 drive, will it make the drive IP55 enclosed rated?
Product Line:
ATV630 and ATV930 Drives with the flange kit.
Environment:
Flange kit only
Cause:
Are the Drives IP55 rated with the flange kit?
Resolution:
If the ATV630 or ATV930 Drive is mounted inside an IP55 enclosure along with the optional IP55 flange kit NSYPTDS5 it allows the main enclosure to keep the IP55 rating with the Drive mounted with the flange kit. Note that the ATV630/930 Drive + flange kit does not provide IP55 protection alone the drive has to be mounted inside an IP55 enclosure.
發佈於: 施耐德電機Taiwan