我们今天能为您提供什么帮助?

What is the part number of jumper bar for BMXFTB2010?

Issue:
Is there a part number of jumper bar for BMXFTB2010?

Product Line:
Modicon X80

Environment:
All serial numbers

Cause:
N/A

Resolution:
The 20-pin jumper bar is not available for spare, and it is only provided for BMXFTB4000.