我们今天能为您提供什么帮助?

How to identify the flow meter version for my ACRC cooling unit Gen 1 and Gen 2

Issue:

Identify old and new flow meters in the ACRC cooling units Gen 1 and 2.

Product Line:

ACRC100, ACRC101, ACRC301S, ACRC301H

Environment:

Selecting the correct flow meter for chilled water Inrow Gen 1 and 2.

Cause:

Identify the flow meters part numbers.

Resolution:

Old flow meter W0N-0278

New flow meter 0J-0N-0303C

Flow meter versions