我们今天能为您提供什么帮助?

Cannot configure the Quantum 140NOC77100 Ethernet IP module.

The Quantum 140NOC77100 Ethernet IP module can be configured in Control Expert or Unity using the attached 'Unity Pro EtherNet/IP Configuration Tool'.

The 'Control Expert' or 'Unity' software must be installed prior to the installation of the 'Unity Pro EtherNet/IP Configuration
Tool'.

'Control Expert' or 'Unity' will need to be started using 'Run as Administrator' in order to open the 'Unity Pro EtherNet/IP Configuration
Tool'.

施耐德電機Taiwan

附件
Ethernet IP Config Soft V1 1.zip [20.68 MB]