Cannot SSH to PowerChute Network Shutdown virtual machine.
Issue:
The user cannot SSH to the PowerChute Network Shutdown virtual machine.
Product:
PowerChute Network Shutdown 4.x, 5.x
Environment:
PowerChute Network Shutdown Linux virtual machine.
Cause:
The SSH service is set incorrectly on the Linux virtual machine.
Solution:
1- Log in to the ESXi host that is hosting the virtual machine.
2- Open a console to the virtual machine and verify that SSH is active.
Run the command systemctl status sshd
If the system reports that sshd is disabled or inactive, enter the command systemctl start sshd
3- After verifying that the service is running, when connecting, an error is posted stating access is denied, or authentication failed. Run the commands listed below to permit the root user SSH access.
For PowerChute VM versions 4.x, 5.0, and 5.1, run the commands:
cp /etc/ssh/sshd_config /etc/ssh/sshd_savedconfig (This command will make a copy of the original sshd_config file.)
echo "PermitRootLogin yes" >> /etc/ssh/sshd_config (This command will add a new line to the sshd_config file permitting root login.)
systemctl restart sshd (This command will restart the sshd service.)
For PowerChute VM versions 5.2 and above, run the commands:
cp /etc/ssh/sshd_config.d/00* /etc/ssh/sshd_config.d/SavedConfig.txt (This command will make a copy of the original 00-complianceascode-hardening.conf file.)
sed -i 's/PermitRootLogin no/PermitRootLogin yes/g' /etc/ssh/sshd_config.d/00* (This command will edit the root log in permissions to allow root to log in over SSH/SFTP.)
systemctl restart sshd (This command will restart the sshd service.)
NOTE: We recommend disabling SSH access when not required.
發佈於: 施耐德電機Taiwan


需要協助?
產品選型工具
快速輕鬆地為您的應用找到合適的產品和附件。
取得報價
立即線上提交您的銷售需求,專業團隊將主動聯繫您。
購買地點
輕鬆在您所在地區找到最近的施耐德電機經銷商。
支援中心
在同一位置找到滿足您所有需求的支援資源。