我们今天能为您提供什么帮助?

How to display DNP3 and/or Modbus protocol addresses in Logic Editor?

If you added DNP3 point numbers and/or Modbus register addresses before selecting the Object Protocol Address(es) in the Logic Editor custom field, you can display those addresses in the SCADAPack x70 Logic Editor:

  1. Go offline in RemoteConnect.
  2. Under My Network, right-click on SCADAPack x70 Controller Settings-DeviceDTM and select Additional Functions>Project Settings.

Display1

  1. Select the Object Protocol Address(es) in Logic Editor Custom Field checkbox.

Display2

  1. Click Ok.
  2. A window will pop up " The Project Settings have been updated. Click the View log File button to see the complete list of changes". and select Close button.

Display3

  1. Open Logic Editor
  2. Under Project > Variables & FB Instances, double click on Derived Variables and view Custom field.

Display4