Error 1720 gets returned during Control Expert install or uninstall
This can occur if the regional setting for the windows clock is incorrectly set or set to use cyrillic letters
It is recommended to ensure that the regional settings for the Windows clock on the PC' is correctly set.
發佈於: 施耐德電機Taiwan