我们今天能为您提供什么帮助?

My Smart UPS Modular Ultra has error code 38B1, 38AB, 38A9 or 38B4

Issue:

My Smart UPS Modular Ultra has error code 38B1, 38AB, 38A9 or 38B4


Product Line:

Smart UPS Modular Ultra


Environment:

All models, all serial numbers


Resolution:

The UPS firmware has been improved to eliminate false detection of these alarms.

Please upgrade the UPS to at least firmware 17.0, then clear all alarms if needed.

In order to upgrade the UPS properly, please use the following FAQ - https://www.apc.com/us/en/faqs/FAQ000261838/

If the alarm returns after upgrading the firmware, please contact support.

施耐德電機Taiwan

附件
SRYL1225UPS_17-0.zip [4.03 MB]