我们今天能为您提供什么帮助?

How to Manually Configure Network Management Card Using the Display of APC Smart-UPS Modular Ultra 5-20kW

Issue:
Need instructions to manually configure the network management card using the display screen on APC Smart-UPS Modular Ultra 5-20kW.

Product Line:
APC Smart-UPS Modular Ultra 5-20kW

Environment:
UPS Models that begin with SRYL5K up to SRYL20K
All Serial Numbers

Resolution:
To manually configure the network management card using the display of your APC Smart-UPS Modular Ultra 5-20kW, follow these steps:

  1. On the home page, select the Configuration menu
  2. Select Network
  3. Set the Address Mode to Manual
  4. Enter the desiredIP Address, Subnet Mask, and Default Gateway
  5. Press OK and confirm to save changes.

The network interface will reboot but this will not affect the connected load to the UPS.

You can also refer to the following video for guidance:


If you experience any problems or require additional help, please contact our customer care center at https://www.apc.com/us/en/support/.