我们今天能为您提供什么帮助?

Easy-UPS BVG - Battery Charger Power

Question:

What is the battery charger power on the Easy-UPS BVG range?

Answer:

The battery charger power on the Easy-UPS BVG range is:

700VA to 1200VA:

14W typical
20W maximum

1600VA & 1200VA:

28W typical
40W maximum