我们今天能为您提供什么帮助?

Configuration log file "Invalid field Id" message in RemoteConnect

After writing a configuration to a x70 device, a user may experience the following System Status Code:

Code: 1012 The configuration contains an unknown attribute. Click Open Configuration Log for details.

Code1012

After clicking the Open Configuration Log button on the Status tab, a messages similar to the following could be seen.

#Rebuilding Configuration from file configuration.rtu at 14:48:54 on 02-06-2025
File Attributes: 12828 bytes, 14:48:54 02/06/2025
File is valid. Rebuilding Configuration
# 733: Invalid field Id: 354073
# 762: Invalid field Id: 352051
# 781: Invalid field Id: 150901
# 823: Invalid attribute for point: 551210
Configuration Rebuild Pass

#732: Unknown configuration table:

Config.log

This message may be displayed when a new feature of SCADAPack RemoteConnect is not available in an older version of firmware. (Various numeric and text values may be displayed).

An unavailable feature may be indicated in this or similar messages by one of the following mnemonics:

DLT = Datalogging

IFW = IP Firewall

MOD... = Modbus scanner

MSF = Modbus Store & Forward

RLU = Role-Based Access Control

RTUS = Device Settings

The remedy is to use the version of firmware that is associated with the version of RemoteConnect.