我们今天能为您提供什么帮助?

FAQ: What are the meanings of Accuracy and Repeatability as found on the ETE datasheet?

Accuracy: The measure of how close a measurement gets to the actual (true) value.

Repeatability: The consistency of the sensor's readings when the same measurement conditions are repeated multiple times. This is an aspect of precision.

Accuracy and Precision