我们今天能为您提供什么帮助?

Geo SCADA: I am unable to delete Historic Data in Geo SCADA 2023

Problem

After upgrading to Geo SCADA 2023, I am no longer able to delete historic data.

Solution

Starting in Geo SCADA 2023, there is a new setting in the server configuration | Historic Configuration | Historic Data dialog titled, “Allow Historic Data to be Deleted”.

historic

If this box is unchecked, Geo SCADA users will not have the ability to delete historic data.

Users may check/uncheck this box and apply the setting with immediate efficacy.  A server restart is not required for this change to take effect.

(Note: a Historic Trend that is open (in ViewX) will need to be closed and then re-opened in order for a change to the ‘Delete Data’ option to be seen.)