我们今天能为您提供什么帮助?

In Vijeo Designer, can I put multiple email addresses under a single alias?

Issue:

Multiple email addresses per alias in Vijeo Designer


Product Line:

Vijeo Designer


Resolution:

Yes, it is possible to have multiple email addresses per alias. You would use the semi-colon to separate the email addresses as shown below

email alias