我们今天能为您提供什么帮助?

ETE - Knowledge - Offer: Installation Examples

EcoStruxure Transformer Expert should ideally be installed in top or bottom oil valves. If there are no oil valves available sensor can be installed in radiator.

Bottom Oil Valve:

1) Before Installation:

Before Installation

1) After Installation:

After Installation

2) Before Installation:

Before Installation

2) After Installation:

After Installation

3) After Installation:

After Installation

Top Oil Valve:

1) Before Installation:

Before Installation

1) After Installation:

After installation

Radiator:

1) Sensor installation in top of radiator

Sensor installation

2) Sensor installed in Pipe to Radiator

Sensor installation