我们今天能为您提供什么帮助?

ETE - FAQ - Offer: What information does the EcoStruxure Transformer Expert Solution provide?

The EcoStruxure Transformer Expert solution provides both raw data and automated health analyses.

The raw includes accurate online monitoring of:

  1. Temperature
  2. Water in oil
  3. Vibration
  4. Acoustic
  5. RF noise


From this data, analyses include:

  1. Operating status
  2. Calculated insulation age
  3. Rate of life-lost over time
  4. Life remaining
  5. Early detection of moisture leaks
  6. Changes in partial discharge
  7. Structural integrity
  8. Industry-wide datasets applied to the specific conditions of the transformer
  9. A fleet-wide view of individual transformer health