我们今天能为您提供什么帮助?

What is the default user name and password for the TM5 Ethernet/IP fieldbus interface module?

Issue:

Default user and password for the TM5 Ethernet/IP interface module

Product Line:

TM5NEIP1


Resolution:

When logging in to Web server for the first time, the default username is admin and the default password is TM5NEIP1. The user is requested to change the password.

NOTE: The only way to gain access to a TM5 EtherNet/IP Fieldbus Interface for which you do not have the password is by performing a Fieldbus interface clear flash memory operation (rotary switch position F0).

(see attached Modicon TM5 EtherNet/IP Fieldbus Interface, Hardware Guide page 37)

施耐德電機Taiwan

附件
TM5-EIP-FBus-Hardware-Guide-EN.pdf [2.24 MB]