我们今天能为您提供什么帮助?

What is the default IP address of the TM5 Ethernet/IP interface module?

Issue:

Default IP address of the TM5 Ethernet/IP interface module

Product Line:

TM5NEIP1


Resolution:

The default IP address of an TM5 Ethernet/IP interface module is determined by converting the last 2 octets in the MAC address. The first 2 octets of the default IP address is fixed at 10.10. x.y , where x.y  is the last two octets of the MAC address

Example:  If the MAC address is 00.80.F4.02.EA.6A then the IP address will be 10.10.234.106

EA Hex = 234 Decimal
6A Hex = 106 Decimal