我们今天能为您提供什么帮助?

DCE 8.x restoring a config backup to a new server with a different mac address causes mac address error

Issue:
DCE 8.x restoring a config backup to a new server with a different mac address causes mac address error

Product Line:
EcoStruXure Data Center Expert

Environment:
DCE 8.x
Configuration backup only

Cause:
DCE sees a config backup incorrectly and when logging into the console using the "apcsetup" user, you can see the mac address error.

Resolution:
It is best to either redeploy DCE with the same mac address or if this is not possible, to create a full or sync backup and restore to the new server using that backup.

This issue is resolved in DCE 9.0