我们今天能为您提供什么帮助?

Number of Sensors Supported by PowerLogic A125

Issue:
How many arc flash sensors can be connected to the A125?

Product:
PowerLogic A125 Arc Flash Protection Relay

Environment:
Switchgear compartments requiring multiple detection points

Cause:
Users need to know sensor capacity for coverage planning

Resolution:
The A125 supports up to four arc sensors (VA1 DA or VA1 EH types) connected via the X2 terminal block