我们今天能为您提供什么帮助?

How to online Install a Brand-New M580 CPU in a hot standby system

When installing a brand-new CPU during the production operation of the system,

-do not connect the network cable between the master and standby CPUs.

After the CPU and CRA are all fully operational, connect the network cable to construct the ring network.

-Alternatively, in accordance with the operating procedure outlined in the user manual,

you can first download the program to the brand-new CPU independently, then integrate the CPU into the on-site control system.

Control Expert manual capture