我们今天能为您提供什么帮助?

How to unstall and connect CMDTOOL to an Interbus master TSXIBY100?

CMDTOOL is a third part software which allows mainly to diagnose an Interbus fieldbus.

This tool can be used also to configure the Interbus Master TSXIBY100.

Most of the people get trouble to get a PC connected to an interbus master.

This action is more difficult with recent PC which doesn't propose a RS232 SubD9pt connector anymore.

In attachment is a step by step procedure to succeed in this operation.

施耐德電機Taiwan

附件
How to connect CMDTOOL on a master.pdf [385.33 KB]