我们今天能为您提供什么帮助?

Is the Profibus Remote Master (TCSEGPA23F14F) compatible with the BMXNOC0401 ?

Issue

Is the Profibus Remote Master (TCSEGPA23F14F) compatible with the BMXNOC0401 ?

Product Line

M340

Environment

Control Expert

Resolution

The PRM is supported only by the M340 BMXNOE01x0, not by the BMXNOC0401 .