我们今天能为您提供什么帮助?

NetBotz 750/755/756: Firmware Update Precaution to Prevent Boot Failure

Issue:

Customers may encounter a “Trying to boot from SPI” message after a firmware update (particularly when updating from version 5.3.5 or later) or following a power interruption. This may result in the unit requiring a replacement.

Product Line:

NetBotz

SKUs affected:

  • Netbotz 750/TAA/EU
  • Netbotz 755/756/TAA/EU

Resolution:

Before starting any firmware update, please execute the following:

If the NetBotz is already on-line:

Verification before upgrade

This can be verified by logging in as root into the command line via console or SSH (shift X when asked to configure) and drop into the command line then type:

root@netbotz862729e5:~# fw_printenv check_rtc

The proper response is:

## Error: "check_rtc" not defined

The incorrect response is:

check_rtc=i2c read 0x68 9 1 0x8000; if itest.b *8000 > 20; then i2c mw 0x68 9 0x1F ; fi

To correct this:

1.  Connect console cable to the appliance

2. Reboot the appliance

3. During the 5 second countdown press any key to enter to enter U-boot command line

4. Type fw_printenv check_rtc to verify if check_rtc exists.

If the output is, ## Error: "check_rtc" not defined, proceed with updating the firmware.

check_rtc_error

If the output is, check_rtc=i2c read 0x68 9 1 0x8000; if itest.b *8000 > 20; then i2c mw 0x68 9 0x1F ; fi

type the following commands to delete the check_rtc line:

·       type: setenv check_rtc

·       type: saveenv

·       type: boot

5. Verify if check_rtc was cleared by executing step 4 and shows## Error: "check_rtc" not defined

6. Proceed with updating the firmware.

Note: Please ensure these steps are strictly followed to help prevent the unit from requiring an replacement.

施耐德電機Taiwan

探索更多
系列:
探索更多
系列: