Note: The LK3 range of switch disconnectors is no longer produced, however to replace it we have the INS range available. Please refer to INS product information, available on our website www.se.com/uk You can also refer to the product selector, available on the same link, for part numbers.
The LK3 switch disconnect products (suitable for load break and isolation applications in accordance with catalogue specifications) are marketed by Schneider Electric specifically in the UK.
As a result, information is not presented on the global web site.
The LK3 (also LK31 prefix on larger versions) covers ratings from 40A Ith through to 1250 Ith in 3 and 4 pole versions.
Please note: Switch disconnect kits (part number LK3***0 or LK31***0) include the switch body that has the same part number as the kit but without the 0 (zero) suffix, e.g. kit LK3AT30 contains body LK3AT3.
Further information covering full product specifications and components, can be found by downloading the PDF catalogue attachment (see link below).
Released for: Schneider Electric UK