No, the integral 18 & 32 motor control circuit breakers are no longer available
The TeSys U range will give a similar, but not exact like for like configuration.
The main differences being the amount of auxiliary contacts the Integral range offered is limited in the TeSys U range.
Also, the model Tesys U power base will give Total coordination.
Model TeSys U
The complete unit is compact & has plug in units for quick change\release.
It can operate on ac or dc supplies:
It can control 1ph & 3ph motors up to 18.5kW depending on model
DOL non reversing
DOL reversing
Star \ Delta configuration
The plug in overload units can give basic up to advanced protection, (Model dependant)
Auxiliary contact slots can be used for control\indication\communication
This basically consists of:
LUB** An independent power base unit
+
LUC** A plug in overload (control Voltage must be stated)
LU** A plug in auxiliary contact block(s)\communication module
The above conformation is only a basic explanation of the range & is intended to give a brief insight into the range
Please call the helpdesk on 0870 608 8 608 for more details or clarification
You can also download the Tesys U catalogue section here: https://www.se.com/uk/en/download/document/A4%20-%20TeSys%20U_EN/
You can also download the Tesys U catalogue section here: https://www.se.com/uk/en/download/document/A4%20-%20TeSys%20U_EN/