undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can you provide longer screws for the ultimate flat plate as my back box is deeper than the screws provided?
M3.5 x 50mm screws are available  and the part number is USCREW50** (Replace ** with the suffix code to denote finish required)

SS  - Stainless steel
PW - Painted White
PN - Pearl Nickel
PB - Polished Brass
PC - Polished Chrome
BN - Black Nickel

M3.5 x 75 mm screws are also available in our Installation Materials Range Part number 3746192

M3.5 x 35 extension studs are also available in our Installation Materials Part number 3746758

Schneider Electric UK

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: