Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a 100A HCN panel with a vertically mounted ``FA`` main breaker be converted from top to bottom feed?
Issue:
How to rotate an HCN panel with a vertically mounted ``FA`` main breaker be converted from top to bottom feed.

Product Line:
I-line Panelboards.

Environment:
Installation.

Resolution:
Yes.

1. Rotate entire panel assembly 180 degrees.

2. Replace factory installed top-feed breaker (FA36100MT) with a standard bottom feed main such as an FA36100.

3. In some cases, the main breaker cover plate (part of interior deadfront) must also be rotated 180 degrees to achieve proper orientation of deadfront labels.



CTA-ID : 2007769

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings