Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement 30A 250V fuse clip for the 8940SSC2007 pump panel?
Issue:
What is the replacement 30A 250V fuse clip for the 8940SSC2007 pump panel Series B?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8940 Pump panels

Resolution:
Order 9422 TC30 fuse clip kit. The kit will include all necessary hardware to replace all the fuse clips.

If Class R rejection is desired order RFK03 kit which includes three rejection pins.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings