Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the terminal nut insert kit that comes with the H frame breakers without lugs?
Issue:
Terminal nut kit for Powerpact H-frame Circuit Breaker

Product Line:
Molded Case Circuit Breakers

Resolution:
The kit number is S37444. The kit includes 3 terminal nut inserts.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings