Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a Powerlogic Monitor or Power Meter available on a I-line panelboard?

Issue:
Available Powerlogic Monitor or Power Meter on a I-line panelboard

Product Line:
I-line panelboard

Environment:
Product Features

Resolution:
Yes, as factory assembled only. Additional gutter space is required. NEMA 1 enclosures only. Refer to FAQ FA97661 for further information.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings