Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the mounting studs in an MH box different than the mounting studs in an HC box?
Issue:
The mounting studs in an MH box are different or equal to the mounting studs in an HC box.

Product Line:
Panelboards

Environment:
Mounting Hardware

Resolution:
For NQOD and NF, the mounting studs are installed in the box as part of the manufacturing process (pierce form) and are not replaceable. I-line and QMB box studs are installed from the back and are held with keeper nuts. I-Line and QMB box studs are replaceable.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings