Issue:
Can an isolated ground bar and neutral be installed on an 800 amp I-Line panel?
Product Line:
I-Line panelboard
Environment:
Application
Cause:
Clarification
Resolution:
The neutral assembly is insulated/isolated as normal in the Digest. An HC2SN neutral kit, for example, can be used as an aluminum isolated ground bar. If a copper neutral bar is required, use part number 40517-424-51.
Revised 4/27/04
CTA-ID : 2014564
Can an isolated ground bar and neutral be installed on an 800 amp I-Line panel?
Product Line:
I-Line panelboard
Environment:
Application
Cause:
Clarification
Resolution:
The neutral assembly is insulated/isolated as normal in the Digest. An HC2SN neutral kit, for example, can be used as an aluminum isolated ground bar. If a copper neutral bar is required, use part number 40517-424-51.
Revised 4/27/04
CTA-ID : 2014564
Released for: Schneider Electric USA