Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the 400, 600, and 800 amp main breaker in the HCM I Line panel?
Issue:
Main breaker part numbers for the 400,600 and 800 amp HCM I Line panel

Product Line:
Square D panelboard.

Environment:
Product Features

Resolution:
The current vertically mounted main breaker in a HCM I Line panel for 400, 600 and 800A is as follows:
The 400A has the LAP36400MB
The 600A has the MGP36600
The 800A hs the MGP36800

Schneider Electric USA

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings