Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is condensation build-up ``normal`` on the inside of a NEMA 3R panelboard NQ?
Issue:
Is condensation``normal`` on the inside of a NEMA 3R panelboard NQ?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboards sold and supported in the USA.

Cause:
Concern over condensation forming inside panelboard enclosures.

Resolution:
Yes, depending on the amount of moisture in the air. The NEMA 3R enclosure in not air-tight and allows outside air to pass throughout the enclosure. As the temperature rises and falls condensation can build up on the inside and out side of the enclosure. A weep hole is provided for drainage of any moisture build-up.












CTA-ID : 2015092

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings