Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the door gasketing be obtained for a Nema 1A, I-Line panelboard enclosure?

Issue:
Loose gasketing material

Product Line:
Panelboards

Environment:
I-Line

Cause:
Repair

Resolution:
Yes, order part number 80106-507-01 and this will have to be ordered per foot. (so customer will need to specify total feet required when ordering, and order must be placed on the Peru Plant) . This goes on the back of the door so a trim with door is required. For a Nema 12 rating use a HC**WP box.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings