Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are stainless steel enclosures available for HCP panelboards?

Issue:
Stainless steel enclosures for HCP panelboards

Product Line:
Panelboards

Environment:
I-Line HCP

Cause:
Nema 4/4X SS Panel Boxes

Resolution:
Yes. NEMA 3R stainless or NEMA 4/4X stainless enclosures can be selected in Product Selectors. (Factory Assembled Only)  However, it is not available for the single row
HCP-SU.  If required, panelboard will have to be configured as HCP double row.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings