Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the lug wire range for HCP235912N and will it accept up to 750KCMIL?
Issue:
HCP235912N will accept 3 conductors larger than 500KCMIL

Product Line:
Panelboards

Environment:
I-line HCP 1200A Panel

Cause:
Needed larger incoming lugs

Resolution:
The actual wire range of the main lugs is (4) #3/0 - 750MCM per phase and neutral. The acceptable wire range per NEC Table 373-6 is (4) #3/0 - 500MCM based on the available wire bending space in the standard enclosure. If incoming cables are larger than 500MCM, an extended end gutter may be required.

NOTE: Extended end gutters are only available on NEMA 1 enclosures. Please refer to the Suplemental Digest or your local distributor for a part number.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings