Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the main terminal lug data for a 600A Main Lug Only I-Line Panelboard?

Issue:
What is the wire range for a 600A Main Lug Only I-Line Panelboard?

Product Line:
I-line panelboards

Environment:
Products used in the United States

Cause:
Product features

Resolution:
The wire range for the 600A MLO is (2) #2-600 kcmil Al/Cu wires. However, the UL listed wire range, based on the wire bending space is (2) #2-500kcmil per phase and neutral.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings