Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can one obtain accessory main lugs to change from main breaker to main lug on an HCN type I-Line panel?

Issue:
Can one obtain accessory main lugs to change from main breaker to main lug on an HCN type I-Line panel?\

Product Line:
Panelboards

Environment:
I-Line HCN

Cause:
Kit for ease

Resolution:
There is no kit available to change the HCN panel from main breaker to main lug.

Note: Effective December, 2014, the HCN style I-Line panelboard was obsoleted. Replace panel with the HCM style.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings