Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can we make a 120 volt only NQ panelboard?

Issue:
120V NQ panelboard Availability

Product Line:
Panelboard

Environment:
NQ

Cause:
Application.

Resolution:
We can make a 120 volt only panelboard as a special. It can be main lug or main breaker type providing that a 1 pole breaker is available for use in the application. The bus bars in a 1 phase NQOD interior will be jumpered to create one continuous bus.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings