Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the trim mounting screws for a NQOD panel 225 amp maximum with a non-hinged trim?
Issue:
What is the part number for the trim mounting screws for a 225A maximum NQOD panel with a non-hinged trim?

Product Line:
NQOD panelboards

Environment:
Maintenance/Installation

Resolution:
I4020513001K is a package of (10) screws.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings