Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does an HC4286WP come with the lock installed?
Issue:
HC4286WP is missing the lock.

Product Line:
I-Line

Environment:
Nema 3R/12 enclosures

Cause:
Lock is missing

Resolution:
The Nema 3R/12 enclosures are shipped with the lock not installed, but is packaged inside the enclosure to prevent damage.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings