Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are replacement lugs available for the Class 9422 Type T 30 amp and 60 amp disconnect switches?
Issue:
Replacement lugs for the 9422T 30 and 60 amp disconnect switches

Product Line:
Disconnect Switches

Environment:
9422 T Disconnect Switches

Resolution:
Yes as outlined below:
For line or load side the standard aluminum lug is part number 40251-016-52. Note: this part number is for a single lug.
For devices with factory form Y157; line or load side copper lug is part number 40256-728-50. Note: this part number is for a single lug.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings