Issue:
Application
Product Line:
Molded Case Circuit Breakers
Resolution:
The breaker has a 5/8" stub shaft with a hole in the middle upon which a handle extension S29313 can be installed on all PowerPacT H frame breakers. If the stub shaft is broken, the breaker must be replaced.
Application
Product Line:
Molded Case Circuit Breakers
Resolution:
The breaker has a 5/8" stub shaft with a hole in the middle upon which a handle extension S29313 can be installed on all PowerPacT H frame breakers. If the stub shaft is broken, the breaker must be replaced.
Released for: Schneider Electric USA