Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do we order PowerPacT H- or J- Frame breakers with and without the handle extensions?
Issue:
Powerpact H- or J- Frame with or without handle extension

Product Line:
Molded Case Circuit Breakers

Resolution:
As of September 2005, breakers are built without handle extensions. Adding suffix YE adds the handle extension. The field installable catalog number is S29313.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings