Isuue:
ATV58 analog input
Product Line:
ATV58
Environment:
All series
Cause:
N/A
Resolution:
No. AI1 can only function as a PI setpoint or a manual speed reference depending on the programming. AI1 can not function as a feedback signal. AI2 is the default PI feedback signal.
If a 0-10V feed back input signal is desired use the Analog I/O Option Card, VW3A58201U or Digital I/O extension card VW3A58202U. AI3 can be used as PI feedback.
Also, it is possible to use a signal converter to change 0 to 10v signal to 4-20 mA and use AI2 for the feedback.
This device standard part number is 31158-297-50 or as with ordering the Econoflex the J09 option.
ATV58 analog input
Product Line:
ATV58
Environment:
All series
Cause:
N/A
Resolution:
No. AI1 can only function as a PI setpoint or a manual speed reference depending on the programming. AI1 can not function as a feedback signal. AI2 is the default PI feedback signal.
If a 0-10V feed back input signal is desired use the Analog I/O Option Card, VW3A58201U or Digital I/O extension card VW3A58202U. AI3 can be used as PI feedback.
Also, it is possible to use a signal converter to change 0 to 10v signal to 4-20 mA and use AI2 for the feedback.
This device standard part number is 31158-297-50 or as with ordering the Econoflex the J09 option.
Released for: Schneider Electric USA


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.