Issue:
Operate I-Line II busway with DC voltages
Product Line:
PTLVB - Busways Power IEC & Nema
Environment:
Nema Busway sold and supported in North America
Resolution:
It can be used with AC or DC voltages up to 600 volts.
Operate I-Line II busway with DC voltages
Product Line:
PTLVB - Busways Power IEC & Nema
Environment:
Nema Busway sold and supported in North America
Resolution:
It can be used with AC or DC voltages up to 600 volts.
Released for: Schneider Electric USA


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.