Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
HCR-U I-Line Panelboard and Bonding Strap with and without the neutral CT?
Issue:
What is the part number or the neutral bonding strap for the HCR-U panelboard with and without the Neutral CT?

Product Line:
PTLVS - LV Functional Enclosures

Environment:
I-Line panelboards sold and supported in the USA.

Cause:
What makes an HCR-U I-Line panelboard service entrance rated?

Resolution:
The items listed below are required for installation of neutral bonding strap with the neutral CT:
1- 80121-082-02- bonding strap
1 - BBV57291 mounting hardware

The 80010-600-01 is for the standard HCRU solid neutral that does not have the CT.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings